Skip to main content
Associate III
June 19, 2025
Question

Problem with ADC2 self-calibration in dual mode

Hello ST experts,

Recently, I was developing a project with STM32H750I microcontroller, I faced a problem with ADC self-calibration HAL function (HAL_ADCEx_Calibration_Start)!
I configured ADC1 and ADC2 in dual simultaneous mode + DMA + Timer with synchronous clock mode for clock Prescaler for both ADCs for better synchronization. I executed self-calibration function for ADC1 and ADC2 individually before activating Timer and DMA. The problem was that the microcontroller cannot finish the process. I checked the process only for ADC1. It was okay for ADC1. When I checked the process only for ADC2, it did not work. Also, I checked if I change timer Prescaler to the asynchronized clock mode, the self-calibration function will work. On the other hand, I miss ADCs synchronization. Therefore, I have to use synchronous mode for Clock Prescaler. Have you faced this problem in your projects? Could you please help me in this issue?

This topic has been closed for replies.

4 replies

Karl Yamashita
Principal
June 19, 2025

It was okay for ADC1. When I checked the process only for ADC2, it did not work. 

You have to be more specific in what you mean by "it did not work"?

Was it that HAL status was not HAL_OK or that it did not return?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate III
June 20, 2025

Hello Karl,
This is the part of my code:
if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY, ADC_DIFFERENTIAL_ENDED)!= HAL_OK)
{
Error_Handler();
}
HAL_Delay(500);
if(HAL_ADCEx_Calibration_Start(&hadc2, ADC_CALIB_OFFSET_LINEARITY, ADC_DIFFERENTIAL_ENDED)!= HAL_OK)
{
Error_Handler();
} 
HAL_Delay(500);
HAL_TIM_Base_Start(&htim3);
HAL_ADCEx_MultiModeStart_DMA(&hadc2, (uint32_t*) ADC_BUFFER, 6);
The microcontroller cannot continue and it seems it got in a infinite loop!
Could you please help me?

Karl Yamashita
Principal
June 20, 2025

So why are you calling this twice?

if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY, ADC_DIFFERENTIAL_ENDED)!= HAL_OK)
{
	Error_Handler();
}
HAL_Delay(500);
if(HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY, ADC_DIFFERENTIAL_ENDED)!= HAL_OK)
{
	Error_Handler();
} 

When you call HAL_ADCEx_Calibration_Start, it calls ADC_Disable.

In ADC_Disable, it's calling HAL_GetTick(). If the System tick isn't working, then it will be stuck forever. But you have to run the debugger and see if uwTick is incrementing or not during the while loop.

 

Are you running internal clock or external clock? Upload your IOC file so we can see your clock settings.

 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source