Skip to main content
Tung Nguyen (晉松)
Associate II
May 29, 2023
Question

Problem with 1us clock signal generation from Timer in STM32G474 EV Board

Hi Everyone. My EV Board use 24 MHz HSE but I used PLL to get with 170 MHz, I also set this frequency for the clock of timer module. I could get 2us periodic signal normal from timer setting however I cannot get 1us periodic signal normally (you can check the prescaler and ARR setting in picture). Is there any MCU limitation or what could be the problem? Thanks a lot for help!

***1us signal generation


_legacyfs_online_stmicro_images_0693W00000bl4r1QAA.png***2us signal generation


_legacyfs_online_stmicro_images_0693W00000bl4rBQAQ.png

This topic has been closed for replies.

6 replies

waclawek.jan
Super User
May 30, 2023

Are you trying to toggle a pin in the timer's interrupt? That may not work simply because of interrupt routine's duration.

JW

Tung Nguyen (晉松)
Associate II
May 30, 2023

Hi JW. Thank you for your reply. My purpose is to create 1us ISR, currently I do the GPIO toggle for the checking corectness of ISR duration purpose only. As your hyper link, look like the ISR take long time to finish itself, and no way to get the correct 1us for timer ISR, right?

waclawek.jan
Super User
May 30, 2023

That of course depends on what code runs in that ISR.

Cube adds unnecessary layers.

Compiler optimization setting also matters.

JW

Tesla DeLorean
Guru
May 30, 2023

Interrupts at 1 MHz are generally not viable, and no other work will get done.

Use the TIM HW modes to toggle a pin associated with a TIMx_CHx directly, or use a PWM Output mode with 50/50 duty.

​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tung Nguyen (晉松)
Associate II
May 31, 2023

Yes. Thank you for your reply. Actually, my target is to create 1us ISR for implement a state machine flow-chart with some if-else loop and also GPIO on and off in-side. The toggle GPIO in the waveforms showed above just the checking signals that I generated to make sure I got 1us or not!