Skip to main content
a7medinf
Visitor II
May 7, 2012
Question

problem when loading program into flash memory pf my STM32VL discovery

  • May 7, 2012
  • 2 replies
  • 532 views
Posted on May 07, 2012 at 23:41

can't download my program

on the STM32F100RBT6B of the discovery board

and a the dialog box of downloading shows no progress of the programming process.

here the picture of problem:

0690X00000603EtQAI.jpg

after clic cancel :

0690X00000603EUQAY.jpg

    This topic has been closed for replies.

    2 replies

    zrafi
    Visitor II
    May 7, 2012
    Posted on May 07, 2012 at 23:46

    I had the same problem. the red LED still blinking showing a communication between STLink and the STM32 device but the dialogbox still showing no progress and nothing happens. is it a hardware problem knowing that i made no hardware modification on the discovery kit?

    frankmeyer9
    Associate III
    May 8, 2012
    Posted on May 08, 2012 at 11:27

    Can you access the Discovery board with the STLink-Utility tool ?

    I did not yet mess much with IAR WB, but make sure you selected the right debug adapter. The STM32VLDiscovery is the 'old' STLink adapter version (V1).