Skip to main content
April 15, 2021
Question

Problem Using Jump_To_Application() in app programming (IAP)

  • April 15, 2021
  • 2 replies
  • 815 views

Hello there.

I'm using a stm32F417VGT6 to perform an IAP in Keil IDE.

in the bootloader, using the Bin file on a SD card, I read executed Binary program and write it on flash memory. then i use  Jump_To_Application() to start the new app. Everything works just fine and we've got no problems.

also if we want to jump to app in the middle of the process in main() (before the flashing new file for sure), it's still OK and application runs fine.

*BUT* when i want to use the jumping function from a timer interrupt callback function or SysTick_Handler() (for example after 20 sec) , the remote app won't work. it Looks like a Hard fault or any type of stucking the code and unfortunately, theres no way to debug because the MCU is not on the bootloader anymore. So i can't jump to app from an interrupt function.

(PS. Note that in this scenario, we don't want to flash the new Binary file. only jumping to the specified SCB->VTOR address from a timer interrupt is needed).

and here's the set of codes i use to perform the jump:

                  JumpAddress = *(uint32_t*) (FLASH_USER_START_ADDR + 4);

                  Jump_To_Application = (pFunction) JumpAddress;

                  Jump_To_Application();   

I would be appreciated if you share your solutions.

or if you needed more details, feel free to ask.

regards

Seyed

This topic has been closed for replies.

2 replies

April 15, 2021

Solved.

the code was making a Hard fault problem was the interrupts priority. in the default CubeMX interrupt priority, All priorities are set to 0. by changing the priority of TIM2 into 2 the jumping was ok from the PeriodElapsedCallback.

Tesla DeLorean
Guru
April 15, 2021

You need to unwind the call stack and NVIC state properly, jumping to entirely different code flow from interrupt/callback is highly problematic.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..