Skip to main content
faradey
Associate
October 2, 2008
Question

Problem TIM3 CH2 PWM Partial remap (PB5) not work

  • October 2, 2008
  • 2 replies
  • 831 views
Posted on October 02, 2008 at 09:48

Problem TIM3 CH2 PWM Partial remap (PB5) not work

    This topic has been closed for replies.

    2 replies

    faradey
    faradeyAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:46

    I want use PWM function on PB.5 - remap TIM3 channel 2 but this code not work.

    I connect pin PB.5 to an oscilloscope and view only high level.

    Code:

    ...

    GPIO_PinRemapConfig( GPIO_PartialRemap_TIM3, ENABLE);

    GPIO_InitTypeDef tmp;

    tmp.GPIO_Mode = GPIO_Mode_AF_PP;

    tmp.GPIO_Speed = GPIO_Speed_50MHz;

    tmp.GPIO_Pin = GPIO_Pin_5;

    GPIO_Init( GPIOB, &tmp );

    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

    TIM_OCInitTypeDef TIM_OCInitStructure;

    TIM_TimeBaseStructure.TIM_Period = 999;

    TIM_TimeBaseStructure.TIM_Prescaler = 0;

    TIM_TimeBaseStructure.TIM_ClockDivision = 0;

    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

    TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);

    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

    TIM_OCInitStructure.TIM_Pulse = 500;

    TIM_OC2Init(TIM3, &TIM_OCInitStructure);

    TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable);

    TIM_ARRPreloadConfig(TIM3, ENABLE);

    TIM_Cmd(TIM3, ENABLE);

    ...

    christophe239955_st
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:46

    Check

    http://www.st.com/stonline/products/literature/es/14574.pdf

    : I2C1 and TIM3_CH2 remapped.

    The I/O port pin PB5 is set to 1 by default if the I/O alternate function output is selected and I2C1 is clocked. TIM3_CH2 cannot be used in output mode.

    Chris.