Skip to main content
mustapha_menhou
Associate II
March 20, 2013
Question

problem STM32-P103 flash loader demonstrator

  • March 20, 2013
  • 42 replies
  • 4992 views
Posted on March 20, 2013 at 19:17

hi

now I

am trying to

achieve

a

basic

equipment

card

STM31

-P103

Olimex

of

(

STM32F103RB

microcontroller

),

I used

the

Flash

loader

demonstrator

program

for

the card (

boot0=1 

boot1

= 0) and i chose COM3, baude=115200, parity=None, Echo=Disable, Time out=10

 

but it always

displays the

following error

:

''no response from the target the boot loader can not be started

thank you for

your help'' 

thank you for

your help.

    This topic has been closed for replies.

    42 replies

    Tesla DeLorean
    Guru
    March 20, 2013
    Posted on March 20, 2013 at 21:48

    The system loader expects even parity. You can test in a terminal program by sending an 0x7F byte and getting an 0x79 response. 9600 8E1 or 115200 8E1 should work.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mustapha_menhou
    Associate II
    March 20, 2013
    Posted on March 20, 2013 at 23:53

    can you

    explain a

    little

    detail

     , 

    because I am

    beginner and

    thank you ???

    Tesla DeLorean
    Guru
    March 21, 2013
    Posted on March 21, 2013 at 01:00

    The BOOT0=High(1) initiate the System Loader stored in the STM32's ROM

    A serial terminal program is something like RealTerm or TeraTerm, allows you to communicate with the attached device via a serial port.

    0x7F is a byte in hex, if you send this byte to the System Loader it should recognized it, and respond with an 0x79 acknowledgement. Doing this is a basic test that the System Loader is there and responsive, if this doesn't work you're not going to get other tools to talk to it either.

    http://www.st.com/web/en/resource/technical/document/application_note/CD00167594.pdf

    http://www.st.com/web/en/resource/technical/document/application_note/CD00264342.pdf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    trevor23
    Associate III
    March 21, 2013
    Posted on March 21, 2013 at 01:56

    Just to add that 0x7F can usually be sent from a terminal by pressing the ''Delete'' key on your keyboard

    mustapha_menhou
    Associate II
    March 21, 2013
    Posted on March 21, 2013 at 10:57

    thank you for

    your help

    but I can not

    to solve

    the problem,

    hyperterminal

    not receiving any

    information

    here is a

    PDF

    that illustrates

    my

    problem?

    ??

    and thank you for

    helping me.

    ________________

    Attachments :

    problem.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0u9&d=%2Fa%2F0X0000000bhp%2FSqidWpeB1a_zLWKI8l.8aP0__i66LPRiKJOLo0lkcsI&asPdf=false
    trevor23
    Associate III
    March 21, 2013
    Posted on March 21, 2013 at 11:17

    Hyper-terminal does not have a binary mode so not a good choice in this case (or any case really). Use Tera Term or RealTerm as suggested by Clive.

    Do you have null modem that you could use to test your serial port using another serial port that you know works? Are you sure the serial port works i.e. you have used it for something else previously with success?

    mustapha_menhou
    Associate II
    March 21, 2013
    Posted on March 21, 2013 at 11:32

    I

    tested

    the port of my

    PC

    by

    Matlab

    I

    shorted

    with

    RX

    and

    TX

    I send

    characters

    after

    I receive this characters.

    mustapha_menhou
    Associate II
    March 21, 2013
    Posted on March 21, 2013 at 12:29

    I

    tested

    several

    speed

    but I can not

    get anything

    except

    a

    speed

    1200

    but I think

    the noise

    Here

    is

    an image that

    shows the

    characters

    received

    ________________

    Attachments :

    bruit.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I13O&d=%2Fa%2F0X0000000bho%2FQTFh5yBIjSv3AvGjVDuRDnpwXFXEBvDSrGKVcEzFGqk&asPdf=false
    mustapha_menhou
    Associate II
    March 21, 2013
    Posted on March 21, 2013 at 13:15

    STM32

    -P103

    card

    from

    Olimex

    uses

    USART2 in

     

    the

    RS232 port and

     

    USART1 in

    UEXT

    .

    I know

    if the problem

    at

    USART

    ???????

    and thank you

    Tesla DeLorean
    Guru
    March 21, 2013
    Posted on March 21, 2013 at 14:43

    Per the document I cited, only USART1 is usable by the System Loader of the STM32F103 chip. You can't use this mechanism easily, use a JTAG programmer.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..