Skip to main content
jlsilicon
Visitor II
January 16, 2014
Question

Problem solved.

  • January 16, 2014
  • 0 replies
  • 603 views
Posted on January 16, 2014 at 09:04

Nothing weird in the ISR.

I used a standard example,

 just added a few Pin toggles to follow with LEDs.

Don't see it entering the ISR during DEBUG Mode at all though.

-

Got it - found the problem !

One of the mcp2551 chips (or both) is not working.

So I use the Diode circuit below, and got rid of the failed mcp2551 chips.

It enters into the ISR properly repeatedly on schedule now !

Data is not always perfect - but can solve that at my ease (via protocols).

Learned Notes:

1) Connecting CAN Tx to Rx on same Chip - will Not work.  It will just continuously Resend without Receiving in the ISR.  If it answered its own message - how could any other Node/Chip answer it then ? 

2) Connecting TxRx to another chip RxTx with common Gnd does not work.

3) Can use Simpler DIODE circuit instead of a CAN chip which works somewhat ok.  Link (2) micros together via a wire connected to the CAN RX lines and Diodes connecting the TX (as a drain) to the same line.  And, using a common Gnd wire. 

  Micro1:                                                 Micro2:

CAN RX <-------+-------------+-------> CAN RX

                          |                   |

CAN TX >--|<--+                  +-->|--< CAN TX

Gnd o-----------------------------------------o Gnd

This gives a lot simpler setup for Debugging.
    This topic has been closed for replies.