Skip to main content
freya17365
Associate III
March 11, 2016
Question

Problem reading SD card

  • March 11, 2016
  • 2 replies
  • 817 views
Posted on March 11, 2016 at 20:08

Hi to all,

I have a big issue with SD cards.

I initialize correctly my sd card, but when I try to read a block, I can read it only the first time.

This is my routine:

=====================

uint32_t MYSD::ReadSector(uint32_t sector, uint8_t *block)

{

    uint8_t t;

    uint16_t i;

    

    

    GPIOA->BRR = 0x01<<SDSS0;    // Set SDSS0 low

    t = CommandAndResponse(SPICMD17, sector);    //Read sector command

    if(t != 0)

    {

        GPIOA->BSRR = 0x01<<SDSS0;    // Set SDSS0 high

        myusart1.PrintString((uint8_t *) ''Cannot read (CMD17)'', ' ', 0);

        myusart1.PrintHex8(t);

        myusart1.PrintChar('\n');

        return 1;

    }

    

    do

    {

        t = sp->Transfer8(0xFF, 0, 0);    // Wait for card response

    }

    while(t == 0xFF);

    if(t != 0xFE)

    {

        GPIOA->BSRR = 0x01<<SDSS0;    // Set SDSS0 high

        myusart1.PrintString((uint8_t *) ''Cannot read (Token response)'', ' ', 0);

        myusart1.PrintHex8(t);

        myusart1.PrintChar('\n');

        return 2;

    }

    

    for(i=0; i<512; i++) block[i] = sp->Transfer8(0xFF, 0, 0);    //Read data

    

    t = sp->Transfer8(0xFF, 0, 1);    // Read CRC

    t = sp->Transfer8(0xFF, 0, 1);    // Read CRC

    GPIOA->BSRR = 0x01<<SDSS0;    // Set SDSS0 high

    

    return 0;

}

=====================

and this is the tesponse:

Iteration 1: CMD17 response 0

Iteration 2: CMD17 response 4

Iteration 3: CMD17 response 0

Iteration 4: CMD17 response 4

Iteration 5: CMD17 response 0

Iteration 6: CMD17 response 4

Iteration 7: CMD17 response 0

Why I can read block in odd iterations and not  in even? The routine is always the same.

Anyone encountered the same problem?

Thank you

Freya

    This topic has been closed for replies.

    2 replies

    viteks
    Visitor II
    March 13, 2016
    Posted on March 13, 2016 at 18:52

    STM32F107? STM32F437?

    Card capasity?

    freya17365
    Associate III
    March 14, 2016
    Posted on March 14, 2016 at 07:47

    STM32F030 at 8MHz

    SPI at 4 MHz (fclk/2)

    Micro SD card capacity 8GB