Skip to main content
pianistjon
Visitor II
June 26, 2014
Question

Problem of STM32f0308 with STEVAL-IDW001v1

Posted on June 26, 2014 at 12:02

to be migrated, sourceId: 11436:74F499D6-C293-4561-BFB5-4F1489999957

    This topic has been closed for replies.

    3 replies

    Nickname306_O
    Visitor II
    October 16, 2014
    Posted on October 16, 2014 at 16:55

    Hi lor.jon,

    Please ensure that you are using SWD instead of JTAG (only SWD connection protocol is supported for STM32F0xx Devices) :

    Project Options --> Debug --> ST-Link Debugger --> Settings --> Debug --> Port --> SW.

    Best Regards,

    Nouha

    armando
    Associate
    March 19, 2015
    Posted on March 19, 2015 at 16:07

    Hi lor.jon, 

    did you resolve your problem?, I have the same issue but with IAR IDE project. I connect the STEVAL-IDW001V1 with the STM32F0 evaluation board and cannot program/flash the microcontroller, have SWD configured as the main debugger in properties. 

    Tesla DeLorean
    Guru
    March 19, 2015
    Posted on March 19, 2015 at 17:07

    The obvious things to look for would be, is the board correctly orientated, is the board powered correctly?

    Does it work if the daughter board is removed?

    Does it work with ST LINK Utilities?

    Does it work if you play with the connect under reset settings?

    Does it work if you jumper BOOT0 High?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..