Skip to main content
Associate II
Feb 5, 2024 9:27 AM UTC
Solved

Problem of porting FreeRTOS to STM32H573I-DK by CubeMX

Hi everyone,

I have a STM32H573I-DK and try to port FreeRTOS without TrustZone to this board by CubeMX but suffered from a problem.

I installed the X-CUBE-FREERTOS, set TIM17 for HAL Tick and SysTick for FreeRTOS.

It will block (or crash?) in vStartFirstTask() after called vTaskStartScheduler().

I have no idea what happened...

Is there problem of my setting ?

Thanks a lot.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 5, 2024 4:57 PM UTC

@EyckHuang wrote:

It will block (or crash?) in vStartFirstTask() after called vTaskStartScheduler().


Are you calling vStartFirstTask() and vTaskStartScheduler()?

You don't need to call them as they are already called by CMSIS V1 or V2.

I'm attaching a simple project with 4 tasks each one is toggling a LED on the disco board created with CubeMx using CMSIS V2.

See attachment.

Hope it helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

5 replies

Associate
Feb 5, 2024 10:33 AM UTC

Hi,EyckHuang,

  I don't have more details to analyze the problem, but I can provide some ideas. I have also encountered such problems. I created many new tasks, and when I started all of them, a hardware default occurred in vStartFirstTask(). I enabled each task one by one and blocked the others. Finally, I discovered the problematic task. Then gradually enable the functions in the task to locate the specific part of the exception.

  Sometimes it's not an issue with the FreeRTOS, but rather a problem with a certain function, even though it hasn't been called.

 

 

EyckHuangAuthor
Associate II
Feb 6, 2024 2:49 AM UTC

Hi Elatewendy,

My problem has been solved and thanks for your shared.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 5, 2024 4:57 PM UTC

@EyckHuang wrote:

It will block (or crash?) in vStartFirstTask() after called vTaskStartScheduler().


Are you calling vStartFirstTask() and vTaskStartScheduler()?

You don't need to call them as they are already called by CMSIS V1 or V2.

I'm attaching a simple project with 4 tasks each one is toggling a LED on the disco board created with CubeMx using CMSIS V2.

See attachment.

Hope it helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
EyckHuangAuthor
Associate II
Feb 6, 2024 2:48 AM UTC

Hi SofLit,

I deployed your example on my board, and it worked fine. Then I found what caused my board crash is printf. I used printf to print some logs to UART1.

But it needs to add link option -specs=nano.specs -specs=nosys.specs if compiled by GCC.

Thanks for your attachment.

Associate
Dec 8, 2025 4:12 PM UTC

I experience the same problem.

But it comes from the TrustZone which was enabled.

I disabled it with CubeProgrammer. And it works.  

Linker options are already set.