Skip to main content
CME
Associate
September 20, 2018
Question

Problem of ADC internal voltage regulator in STM32H743IIT

Hello ,

When I debug the ADC1, In function HAL_ADC_Init(), it was blocked in " Enable ADC internal voltage regulator " because of the failure of verification ADC voltage regulator,.Here I attached the original code:

if  (HAL_IS_BIT_CLR(hadc->Instance->CR, ADC_CR_ADVREGEN))

  {

  /* Enable ADC internal voltage regulator */

   SET_BIT(hadc->Instance->CR, ADC_CR_ADVREGEN);

  /* Delay for ADC stabilization time                          */

  /* Wait loop initialization and execution                      */

  /* Note: Variable divided by 2 to compensate partially              */

  /*    CPU processing cycles.                            */

   wait_loop_index = (ADC_STAB_DELAY_US * (SystemCoreClock / (1000000 * 2)));

  while(wait_loop_index != 0)

  {

    wait_loop_index--;

  }

  }

 /* Verification that ADC voltage regulator is correctly enabled, whether  */

 /* or not ADC is coming from state reset (if any potential problem of    */

 /* clocking, voltage regulator would not be enabled).            */

 if (HAL_IS_BIT_CLR(hadc->Instance->CR, ADC_CR_ADVREGEN))

 {

  /* Update ADC state machine to error */

  SET_BIT(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL);

  /* Set ADC error code to ADC IP internal error */

  SET_BIT(hadc->ErrorCode, HAL_ADC_ERROR_INTERNAL);

  tmp_hal_status = HAL_ERROR;

 }

I'm not sure whether the ADC1 is damaged or not.

look forward to you answers.

Thanks!

This topic has been closed for replies.

2 replies

HPERNET
Associate
May 3, 2022

Hello,

It's seams that I have the same issue did you find any solution ?

Thanks

KKong.3
Visitor II
May 25, 2022

In my case, calling

__HAL_RCC_ADC_CLK_ENABLE()

prior to

HAL_ADC_Init()

fixed the issue.

I'm using STM32L4.