Skip to main content
gustavo2
Associate
June 9, 2014
Question

Problem in CAN1 of STM3220G-Eval

  • June 9, 2014
  • 2 replies
  • 658 views
Posted on June 09, 2014 at 15:52

Hi, I have faced problems using CAN1 in evaluation board STM3220G-Eval. I've used the CAN Network example project of STM32F2xx STD LIB. I have two STM3210C-Eval and one STM3220G-Eval. So I tested the network between STM3210C-Eval boards and it worked. I tested the network between STM3210C-Eval and STM3220G-Eval but it didn't work. So, I tried to use CAN2 instead of CAN1 in STM3220G-Eval (by change the definition USE_CAN1 to USE_CAN2 and setting jumpers JP3 and JP10 correctly) and it worked. I've searched for similar problems in the forum but have no success.

Can anyone help me? What is wrong with this?

#stm3220g-eval #can1
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
June 9, 2014
Posted on June 09, 2014 at 21:24

I don't have an STM3220G-EVAL, but have the STM3240G model, can't say I've tried CAN on it but will double check the schematic for jumpers/options/conflicts.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
gustavo2
gustavo2Author
Associate
June 9, 2014
Posted on June 09, 2014 at 22:08

Thanks for attention, clive1, but the problem was on me using the wrong connector. Differently from STM3210C-Eval, STM3220G-Eval doesn't have one connector for each CAN. The same connector is shared for CAN1 and CAN2. :(

Sorry for this.