Associate III
Jan 9, 2017 7:37 AM UTC
Question
Problem Encoder on STM32F071
- 5 replies
- 1256 views
Posted on January 09, 2017 at 08:37
Hi,
I'm using XCube for init a SMT32F071CBT6 with Keil V5, I need to use the encoder periphery. (ALL to the last version)
In attachment three file. The project and the 2 file modify after generation.
I've use 4 alternative pins, because the other are use by an other periphery.
When start the encoder the 2 pins become output and go Low. Why?
After this command:
HAL_TIM_Encoder_Start(&htim3, TIM_CHANNEL_ALL);
I' ve try with tim1 with exactly the same code with no problem.
Please help me.
#encoder-stm32f0