Problem BlueNRG-1 and ST-Link Debugger under Eclipse
I have the STEVAL-IDB007V1 DK with the BlueNRG-1 chip.
First I work with IAR Embedded workbench and it works fine.
Today I install Eclipse with the system workbench for STM32 and port the Project for eclipse.
It works fine but the problem is to use the debugger (ST-Link V2) and I don´t know why.
I have install the openocd for GNU ARM Eclipse and add it to the Debug Configuration.
But every time I start debugging, I get the failure 'Error while launching command: gdb -- version
Have anyone an idea ?
In the Debug Configuration which Config options the BlueNRG-1 Chip needed ?