Skip to main content
guyvo67
Associate III
October 28, 2009
Question

priority grouping

  • October 28, 2009
  • 4 replies
  • 1640 views
Posted on October 28, 2009 at 11:29

priority grouping

    This topic has been closed for replies.

    4 replies

    guyvo67
    guyvo67Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:27

    Hi,

    As this topic still confuse me a bit maybe you guys can help me get ride of it ;)

    In the case of eg STM32F103RET there are 4 bits implemented as interrupt priorities. ( In theory this arm core can have up to 8 bits ) Which means that I have 16 different levels of priorities. Suppose that I don't want to have sub-priorities and want to work with the full 16 levels of pre-emption only, are the following assumptions correct:

    7 6 5 4 3 2 1 0

    x x x x 0 0 0 0 (-> 4 lowers always zero )

    group 0 : preemption [7-1] sub [0]

    --> according to the book ''definitive guide to arm cortex page 120'' this could not be implemented depending on the core, is this the case with ST devices ?

    group 1 : 7.1 indicates seven bits of pre-emption priority, one bit of sub priority ( out of technical reference manual )

    So if I take group 1 in the case of 4 bits priority implemented I have only 16 level of pre-emption and none sub levels ?

    So in fact group 1 until 4 will have the same impact. As soon as I'll take group 5 I will have 8 level of pre-emptions and 1 sub level and so on correct ?

    Thanks

    -G

    guyvo67
    guyvo67Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:27

    Ok thanks,

    So if I got it well pri-group 4 is the minimum we can set for ST device according the document so having only 16 pre-emptions without sub-pri isnt't possible as we can see in the binary point mask:

    group 4 0b100 0bxxx.y [7:5] [4] 8 2

    group 5 0b101 0bxx.yy [7:6] [5:4] 4 4

    group 6 0b110 0bx.yyy [7] [6:4] 2 8

    group 7 0b111 0b.yyyy None [7:4] 1 16

    Out of the comment from NVIC_PriorityGroupConfig in the nvic file which is not what's in that document ( v2 :(

    - NVIC_PriorityGroup_0: 0 bits for pre-emption priority 4 bits for subpriority

    - NVIC_PriorityGroup_1: 1 bits for pre-emption priority 3 bits for subpriority

    - NVIC_PriorityGroup_2: 2 bits for pre-emption priority 2 bits for subpriority

    - NVIC_PriorityGroup_3: 3 bits for pre-emption priority 1 bits for subpriority

    - NVIC_PriorityGroup_4: 4 bits for pre-emption priority 0 bits for subpriority

    Out of the main.c interrupt priority example file which follows the comment above:

    /* Configure one bit for preemption priority */

    NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);

    So it's still not clear to me because the document doesn't say anything of pri-group 0-4 while the source code does. But there's a lot of shifting done in the NVIC init code I saw like:

    tmppriority = (0x700 - (SCB->AIRCR & (u32)0x700))>> 0x08;

    tmppre = (0x4 - tmppriority);

    tmpsub = tmpsub >> tmppriority;

    .....

    Maybe this is the reason why the grouping isn't quit like the specs tell us. I didn't go into details (debug) to finger it out.

    -G

    [ This message was edited by: guyvo67 on 26-10-2009 12:50 ]

    [ This message was edited by: guyvo67 on 26-10-2009 18:55 ]

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:27

    Hi,

    You can refer to STM32 Implementation of the Cortex-M3 in this document ''STM32F10xxx Cortex-M3 programming manual''

    PM0056 -

    http://www.st.com/stonline/products/literature/pm/15491.pdf

    Cheers,

    STOne-32.

    tomas23
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:27

    ST-One, I agree that Library 3.0 is much more confusing than 2.0, because it doesn't offer any parameter combinations or options for subpriority.