Skip to main content
relaxe
Associate III
September 15, 2009
Question

Pricing of the various IDE/tools for STM32

  • September 15, 2009
  • 31 replies
  • 11194 views
Posted on September 15, 2009 at 20:02

Pricing of the various IDE/tools for STM32

    This topic has been closed for replies.

    31 replies

    tiagomesser
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:02

    I'm using a STM Primer 1.

    I use opensourcery lite (free) with openocd and eclipse.

    Both in Linux and Windows.

    It took me a much more time to set it up then I would have liked.

    But, I think most of the time was spent because my lack of knowledge on things like Makefile and linker script.

    I started with openosourcery about a year ago. Bach then, it was quite more difficult to find examples and things alike. At least it seemed.

    I've used Ride a little while before changing to Eclipse and Eclipse seems more `configurable` then Ride.

    I don't use many plugins for Eclipse, but, I quite sure they could be useful.

    For the JTAG, I planning to use a adaptation of Joern Kaipf's OOCDLink that states being compatible with openocd.

    http://www.joernonline.de/contrexx2/cms/index.php?page=126

    Cheers Brothers,