Question
Precise frequency measurement with STM32F3
Posted on October 20, 2015 at 15:51
Hi, all.
Could you please recommend the best way to do that using STM32 Timers? Input signal is a 5-10 kHz 3V sine-wave, and high-stable TCXO 12 MHz is used for MCU clocking. Measurement should be done with 1E-3 Hz resolution or better, within no more than 5 seconds. Well, curetnly I look to use TIM2 32-bit timer in Input Capture mode with input signal connected to COMP1, and comparator output tied internally to TIM2_CH4 for input/capture. Questions: 1. How to acheive best resolution for frequency measurement? 2. What is the best way to use STM32 timers for this project? #stm32f #timers