Skip to main content
Steven Bébin
Associate III
April 15, 2020
Question

Power supply without regulator

  • April 15, 2020
  • 6 replies
  • 1386 views

Hello,

I am currently working on my end of year project. I first realized my project under a development kit then now I realize the PCB.

I am currently facing a problem. I have an STM32L073RZ which I must supply. As a power supply, I have a Li-SOCl2 accumulator. The battery output voltage is 3.67V in open circuit and 3.6V at 1mA. The supply voltage of the microcontroller is 1.65V to 3.6V.

That's very fair, so I was thinking to use a 3.3V regulator. But the problem is that I have not found a regulator with low consumption. The lowest consumption I found is 40uA, it is very small but it halves the autonomy of my project !

So I wondered if it was possible not to use a regulator and directly power it with the accumulator. Knowing that the accumulator has a nominal voltage of 3.6V and at the end of discharge of 2V.

Thanks,

Steven

This topic has been closed for replies.

6 replies

MViei.1
Associate
May 5, 2022

I would have the same question

MasterT
Lead II
May 5, 2022

MCP1702 - 2 uA

AP7381 - 2.5 uA

Bad idea to not use LDO voltage regulator,

LCE
Principal II
May 5, 2022

... and many more, check the TI LDOs, they have some with Iq < 1µA.

NEVER connect the battery directly!

Peter BENSCH
ST Technical Moderator
May 5, 2022

The STLQ020 might be an interesting alternative: 2-5.5V, 200mA, typ Iq=0.3µA

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LCE
Principal II
May 5, 2022

:) Looks good, but no samples or at distri. available in SOT23-5, adj. or 3.3V :(

Just starting a new project where I could use these, too.

MViei.1
Associate
May 5, 2022

could you tell me why it is a bad idea? sorry really new here