Skip to main content
Slina
Associate III
Dec 3, 2020 8:17 PM UTC
Solved

Power supply scheme for STM32H750

I'm working on PCB with two MCUs, and I'm not sure how to connect power supply lines. Even after reading the datasheet and RM0433, I still find it confusing. Like, which one of the VDD33USB or VDD50USB should I connect and why? Do I connect both? Or do I need to connect VDDLDO? Or VBAT, if I don't plan to use battery and what to do with that pin in that case? Or do I need to connect any of USB VDDs if I'm not using USB or I can keep it floating? Or can I connect the same power supply on all 3.3V power lines? Or can I keep floating analog power input, and use on-chip one?

Is there a nice document to explain it all in details? I was working with SILab MCUs before and the document simply had all scenarios, saving me the trouble of experimenting.

This topic has been closed for replies.
TDK
TDKBest answer
Dec 3, 2020 8:36 PM UTC

This is a better document which describes the required hardware layout:

https://www.st.com/resource/en/application_note/dm00337873-getting-started-with-stm32h74xig-and-stm32h75xig-hardware-development-stmicroelectronics.pdf

That answers most if not all of your questions. If you have questions after reading that, feel free to ask.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
Dec 3, 2020 8:36 PM UTC

This is a better document which describes the required hardware layout:

https://www.st.com/resource/en/application_note/dm00337873-getting-started-with-stm32h74xig-and-stm32h75xig-hardware-development-stmicroelectronics.pdf

That answers most if not all of your questions. If you have questions after reading that, feel free to ask.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Slina
SlinaAuthor
Associate III
Dec 3, 2020 8:43 PM UTC

Awesome! It even has crystal connection schematics. I never would have found that document by myself.

Thanks a bunch.

Piranha
Principal III
Dec 3, 2020 9:37 PM UTC

For oscillators there is also AN2867.