Skip to main content
Rahimi.Meysam
Associate III
September 22, 2015
Question

pointer

  • September 22, 2015
  • 3 replies
  • 877 views
Posted on September 22, 2015 at 18:24

Hello. 

i have this structure definition:(ex)

structure example_str

{

int a[10];

int b[10];

}

and a function with this definition:

void test(example_str *temp);

 i want to change the value that pointer temp is locating with out using another variable to define.

(not to do like this:

example_str test = * temp.

test.a[1] = 10 ;

)

i want to define arrays value directly.

I would be very thankful if everybody help me.

thank you

#pointer
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    September 22, 2015
    Posted on September 22, 2015 at 18:37

    Not 100% sure of what the question is, let's start with something that makes sense and discuss from there.

    typedef struct _example_str {
    int a[10];
    int b[10];
    } example_str;
    void test(example_str *temp, int x)
    {
    temp->a[1] = x;
    }
    int main(void)
    {
    example_str foo = { 0 }; // cleared
    example_str bar = { 0 }; // cleared
    test(&foo, 11);
    printf(''%d
    '', foo.a[1]);
    test(&bar, 22);
    printf(''%d
    '', bar.a[1]);
    while(1);
    return(0);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    September 22, 2015
    Posted on September 22, 2015 at 18:40

    Or are you looking to do this?

    example_str foo = { {1, 2, 3}, {4, 5, 6} }; 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Rahimi.Meysam
    Associate III
    September 23, 2015
    Posted on September 23, 2015 at 07:46

    Thank you Clive. In this post you answer me clearly and problem solved.

    thank you again..