Skip to main content
Associate III
February 28, 2026
Solved

Poblem with ADC + DMA + Timer in STM32H745

Hello ST experts,
I configured an STM32H745 dual core to read data from ADC1/ADC2 in dual mode. I dedicated the M7 core to initialize ADCs, timer and DMA. But after running the code it seems that the ADC is not working either DMA.  
I used the similar code on the STM32H750 single core. The code is correct.
I think I have to configure extra settings for dual core such as managing the memory. Could you please help me.
The DMA is in circular mode with "Word" data length.
TIM2 triggers the ADCs.
 

TDK
TDKBest answer
March 2, 2026

Either post your code or go off one of the many existing examples for this chip.

DMA is not working on STM32H7 devices - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."

8 replies

TDK
March 1, 2026

There's no reason the single core code can't work on the dual core device. Recheck your assumptions. Ensure DMA buffer is somewhere the DMA can access.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
March 2, 2026

Hi,
 Thanks for response. How can I define a buffer with DMA access? Could you please give some suggestion? I am using Keil IDE.

 

mƎALLEm
ST Technical Moderator
March 2, 2026

@Davood_Kesha 

H750 and H745 have the same RAM memory size at the same address location. To me it should work if it is working on H750. 

From which side you are using ADC? CM4 or CM7?

How did you test your case? in debug mode? if yes, CM4 is in low power mode at start up?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
TDKBest answer
March 2, 2026

Either post your code or go off one of the many existing examples for this chip.

DMA is not working on STM32H7 devices - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."