Skip to main content
var2
Associate II
February 19, 2015
Question

Poblem programming stm32f334 witn the flash loader demo 2.7.0

  • February 19, 2015
  • 3 replies
  • 923 views
Posted on February 19, 2015 at 09:09

I can program the stmf32f334 chip without problem with the  desktop version ''FlashLoaderDemo.2.7.0'' - it is Ok.

But the command line version gives error:

''The instruction of ''0x7c911699'' referenced memory of ''0x00000000''. The memory could not be ''read''.''

I checked with the scope. The  bootloader dialog starts Ok. PC sends 0x7F, receives 0x79.

My boot.bat file is below:

''c:\Program files\STMicroelectronics\Software\Flash Loader Demo\STMFlashLoader.exe'' ^

 -c --pn 6 --br 9600 --co ON -Rts --Hi -Dtr --Hi -Dtr --Lo -i STM32F3_34_03_64K ^

 -e --all -d --fn .\Release\F334_nucleo_HRTIM.hex ^

 -Rts --Lo -Dtr --Hi -Dtr --Lo

I try to change the baudrate, no difference.

The chip name STM32F3_34_03_64K is correct.  The desctop version shows

it.

Great thanks for help,

Varuzhan

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    February 19, 2015
    Posted on February 19, 2015 at 12:04

    Sounds like a Windows error, the source is supplied review/debug.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    var2
    var2Author
    Associate II
    February 23, 2015
    Posted on February 23, 2015 at 11:16

    I somebody from ST watches this forum, I need an answer from him, or

    any person, who know the problem.

    AvaTar
    Senior III
    February 23, 2015
    Posted on February 23, 2015 at 14:09

    I wouldn't put too much hope in an answer from ST here...

    ''The instruction of ''0x7c911699'' referenced memory of ''0x00000000''. The memory could not be ''read''.''

     

    That sounds like an ''evil'' NULL pointer reference, probably because of a un-checked return value from some resource allocation function (just a guess). ST might not have tested it on all relevant versions of Windows (including 32/64-bit variants !).