Skip to main content
qwer.asdf
Senior
Oct 23, 2015 12:43 PM UTC
Question

PLL Settings

Posted on October 23, 2015 at 14:43

Hi, is there any difference how exactly I'm getting the desired clock speed on SYSCLK through PLL? For example, let's say I want to have 48MHz on SYSCLK on STM32F407, using a 8 MHz HSE and the PLL. One way of doing it would be this:

HSE = 8MHz

M = 8

 

N = 384

 

P = 8

 

Q = 8

 

--------

 

SYSCLK = 48MHz

Another way of doing it would this:

 

HSE = 8MHz

 

M = 4

 

N = 96

 

P = 4

 

Q = 4

 

--------

 

SYSCLK = 48MHz

So my question is: is one of these two ways better than the other (i.e. lower jitter, or lower power consumption), and why?

Thank you.
    This topic has been closed for replies.

    11 replies

    mikael239955_stm1_st
    Associate III
    Oct 24, 2015 11:26 PM UTC
    Posted on October 25, 2015 at 01:26

    There are numeror bugs in CUBE that's why i only use it for pin mapping and even that dont work 100% depending device you are selecting and it has from the start and it is with the

    latest release.