Question
PLL_Q for USB
Posted on November 18, 2016 at 04:52
STM32L476RG on Nucleo - Porting over the example from EVAL board with 8Mhz Crystal
STM32CubeL4 - HAL demo. If using the HSE with an input source of 8Mhz supplied by STlink, 1. I believe I need to set HSEBYP = 1 for EXTERNAL CLOCK instead of EXTERNAL CRYSTAL. Right? 2. Shouldn't the PLL_Q setting be 6? (6 x 8000000 = 48 MHZ) HAL demo for EVAL and PLL has setting of 4 while the schematic shows again, an 8 MHZ crystal.. /* Select PLLSAI output as USB clock source */ PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB; PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLLSAI1; PeriphClkInitStruct.PLLSAI1.PLLSAI1N = 24; PeriphClkInitStruct.PLLSAI1.PLLSAI1Q = 4; // ?????????PeriphClkInitStruct.PLLSAI1.PLLSAI1P = 1; PeriphClkInitStruct.PLLSAI1.PLLSAI1M = 1; PeriphClkInitStruct.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_HSE; PeriphClkInitStruct.PLLSAI1.PLLSAI1ClockOut= RCC_PLLSAI1_48M2CLK;