Skip to main content
ark2
Associate II
November 9, 2022
Solved

Please tell me how to load the project into stm32

I ran stm32 with cubemx and iar to execute the project, but I have to remove the st-link line and execute it

If I take out the line, the project can't be executed, so how can I only connect the board and power to run the project?

download active application -> download file

I tried it the above way, but it doesn't work when I turn it off and on

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
November 9, 2022

If this is a custom board make sure BOOT0 is pulled low.

​

H​ave places where it dies in while(1) loops silently output more useful reporting or set GPIO or LEDs so you can debug the issue without a debugger attached.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
November 9, 2022

If this is a custom board make sure BOOT0 is pulled low.

​

H​ave places where it dies in while(1) loops silently output more useful reporting or set GPIO or LEDs so you can debug the issue without a debugger attached.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ark2
ark2Author
Associate II
November 10, 2022

Downloading but server source did not work.

Since you wrote the answer, I'll post that it's the best.