Skip to main content
KHe.1
Associate
Mar 16, 2020 5:37 PM UTC
Solved

Please Help!! Why am I not able to setup ADC on STM32F030?

I am trying to setup the ADC channel on PA0. I have first set the pin mode to additional function. Then I have followed the examples provided in the reference manual. However, it doesn't turn on anything, either the calibration or the enable. It is not even selecting channel 0. Am I missing something or did something wrong? This is my ADC related code below:

int main()
 
{
 
	//Set PA0 to Additional function mode
 
 GPIOA->MODER |= (3 << 0) ;
 
 
	//Ensure ADC is Disabled
 
	if ((ADC1->CR & ADC_CR_ADEN) != 0)
 
 ADC1->CR &= (uint32_t)(~ADC_CR_ADEN);
 
 
	//Start ADC Calibration
 
	ADC1->CR |= ADC_CR_ADCAL;
 
	//Wait for ADC Calibration to Complete
 
	while ((ADC1->CR & ADC_CR_ADCAL) != 0) 
	{
	}
 
 
	//Wait for TIM14 is Enabled
 //TIM14 is used as a forever interrupt loop in my while function as a clock
	while ((TIM14->CR1 & TIM_CR1_CEN) == 0)
	{
	}
 
	
 //Select TIM14 by writing 00 in CKMODE
	ADC1->CFGR2 &= (~ADC_CFGR2_CKMODE);
 
	//Enable ADC
	ADC1->CR |= ADC_CR_ADEN;
	while ((ADC1->ISR & ADC_ISR_ADRDY) == 0)
	{
 }
 
	//Enable Continuous Mode
	ADC1->CFGR1 |= ADC_CFGR1_CONT;
 
	//Select Channel 0
	ADC1->CHSELR |= ADC_CHSELR_CHSEL0;
 
	//Select Sampling Mode, TODO: MAY NEED TO ADJUST LATER
	ADC1->SMPR |= ADC_SMPR_SMP_0 | ADC_SMPR_SMP_1 | ADC_SMPR_SMP_2;
 
	//Disable External Trigger
	ADC1->CFGR1 &= (~ADC_CFGR1_EXTEN);
 
	//Wait for ADC is Ready
	while ((ADC1->ISR & ADC_ISR_ADRDY) == 0)
	{
	}
 
 
 
	while (1)	
	{
 
 //Start Conversion
	ADC1->CR |= ADC_CR_ADSTART;
 
	//Fetch Converted Data
	ADC_Data = ADC1 ->DR;
 
 }
 
}
 
 
 

Thank you!

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Mar 17, 2020 12:15 AM UTC

You need to enable clock for each peripheral in RCC.

See examples at the end of RM.

Also the timer's CR1.CEN need to be set explicitly.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
Mar 17, 2020 12:15 AM UTC

You need to enable clock for each peripheral in RCC.

See examples at the end of RM.

Also the timer's CR1.CEN need to be set explicitly.

JW

KHe.1
KHe.1Author
Associate
Mar 17, 2020 1:15 PM UTC

Thank you @Community member​ ! It is all set now.

I thought I only need to setup ADC Clock Mode at CKMODE in ADC_CFGR2.

I added the following code and it works now.

	//Enable ADC Interface Clock
	RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;
 
	//Enable HSI14 Clock
	RCC->CR2 |= RCC_CR2_HSI14ON;
	//Wait for HSI14 Clock to be Ready
	while ((RCC->CR2 & RCC_CR2_HSI14RDY) == 0);