Please explain DMA requests for multiple timer channels on the same stream
On an STM32F4, I am using a timer in IC mode using a DMA transfer. I'm able to do this by setting up and using HAL_TIM_IC_Start_DMA. For a given timer channel, the "DMA request mapping" table in the datasheet shows which stream is connected to which timer. For example, DMA2 stream 1 is connected to TIM1_CH1 on channel 6.
Interestingly, for DMA2 Stream 6 channel 0, the datasheet says it's connected to TIM1_CH1, TIM1_CH2, and TIM1_CH3. What does this mean exactly? Will it trigger a DMA transfer when any one of those three channels has an event? Am I right in assuming there is no way to know which channel triggered the DMA transfer?