Skip to main content
antonius
Associate III
July 28, 2019
Question

Please correct my function ?

  • July 28, 2019
  • 4 replies
  • 705 views

Dear Member,

I'm confused between pointer and array,

Please correct me :

void sim7600_modem(char *SIM_TxBuffer)

{

   printf("sim7600_modem ATI\r\n");

   //Clear buffer

   HAL_UART_Transmit_IT(&huart1,(uint8_t*)&aTxBuffer4, sizeof(aTxBuffer4));

   HAL_Delay(5);

   HAL_UART_Transmit_IT(&huart1,(uint8_t*)SIM_TxBuffer, sizeof(SIM_TxBuffer));

   HAL_UART_Receive_IT(&huart1, (uint8_t *)&SIM900.rxBuffer,1);

}   

on main :

sim7600_modem("ATI\r");

thanks

This topic has been closed for replies.

4 replies

S.Ma
Principal
July 28, 2019

char *SIM_TxBuffer;

sizeof(aTxBuffer))

strings are null terminated, use it to calc the length.

Compiler will not simply even if main is in the same code file as the function...

JChau
Associate II
July 28, 2019

I don't know how do you manage aTxBuffer, but I suspect that may be another point of failure.

First, Array is not pointer, pointer is not array

char* a = "Test string", int* b;
sizeof(a) // is 4
sizeof(b) // is also 4
//sizeof gives you size of the pointer, not the data it points to
char c[] = "Test string";
sizeof(c) // is 12, it is the same as sizeof(char[12]), which is size of the array itself
strlen(a) //is 12 too, this is a function that counts the length of a string

You can simply replace sizeof(SIM_TxBuffer) with strlen(SIM_TxBuffer) for simpler code, but I prefer passing length as a parameter for better optimization on constant length commands.

void sim7600_modem(char *SIM_TxBuffer, size_t length)
{
 printf("sim7600_modem ATI\r\n");
 //Clear buffer
 HAL_UART_Transmit_IT(&huart1,(uint8_t*)&aTxBuffer4, sizeof(aTxBuffer4));
 HAL_Delay(5);
 HAL_UART_Transmit_IT(&huart1,(uint8_t*)SIM_TxBuffer, length);
 
 HAL_UART_Receive_IT(&huart1, (uint8_t *)&SIM900.rxBuffer,1);
} 
 
const char command[] = "ATI\r";
sim7600_modem(command, sizeof(command));

antonius
antoniusAuthor
Associate III
July 29, 2019

const char command[] = "ATI\r";

can not be changed to variables ?

JChau
Associate II
July 29, 2019

I do not quite understand what do you mean cannot be changed to variables, if it cannot be a variable, you can do either

sim7600_modem("ATI\r", 4);

or just use strlen()

#include <string.h>
void sim7600_modem(char *SIM_TxBuffer)
{
 printf("sim7600_modem ATI\r\n");
 //Clear buffer
 HAL_UART_Transmit_IT(&huart1,(uint8_t*)&aTxBuffer4, sizeof(aTxBuffer4));
 HAL_Delay(5);
 HAL_UART_Transmit_IT(&huart1,(uint8_t*)SIM_TxBuffer, strlen(SIM_TxBuffer));
 
 HAL_UART_Receive_IT(&huart1, (uint8_t *)&SIM900.rxBuffer,1);
} 

but to my understanding, even you simply supply a constant ("ATR\r"), compiler will still convert it to a variable because, well, that string still need a place to be stored, so

sim7600_modem("ATI\r", 4);

will still be compiled as something like

const _A = "ATI\r";
const _B = 4;
sim7600_modem(_A, _B);