Placing data at a specific section causes extreme size increase
Hi,
I am trying to have data at a specific location in flash. To do this I have defined my section in the linker script as follows:
.info_data 0x08004674 :
{
. = ALIGN(4);
KEEP(*(.info_data))
. = ALIGN(4);
} >FLASHwith FLASH starting at 0x0800 0000 and having a size of 18KB.
The data to be placed is defined in a .h file like this:
uint32_t volatile const info __attribute__((section(".info_data"))) = 0x12345678;This works, but it causes the file to be significantly larger.
If I don't inlcude the data, the hex file ends at address 0x0800 3820, so well within the 18 KB range. However including this data causes the linker to stop with the main code at 0x0800 307C, places info_data at 0x0800 4674 and then places the rest of the code from 0x0800 4678 to 0x0800 4E1C. (I extended FLASH to 20KB size, to test this).
Why does the linker leave so much empty space between the start of info_data? Is there anything I can do to minimize this? I tried with -fno-function-sections and -fno-data-sections but that didn't help.