Skip to main content
dion
Associate II
April 2, 2012
Question

pin VBUSON stm32-h107

  • April 2, 2012
  • 2 replies
  • 724 views
Posted on April 02, 2012 at 22:40

Hello to all,

i have a question regarding stm32-h107 : in order to use feature usb on the go, should i connect pin USB_VBUSON to Vdd?

Best Regards,

Dion

    This topic has been closed for replies.

    2 replies

    alok472
    Associate
    April 3, 2012
    Posted on April 03, 2012 at 06:28

    Better refer to Evaluation board schematics.

    The VBus needs to be connected to the USB Power Switch output and also to Vbus of the STM32F105.

    The Power switch is needed for using the MCU in host mode and direct connection to Vbus is needed to use in device mode.

    The Power-switch enable needs to be controlled by mcu.

    dion
    dionAuthor
    Associate II
    April 3, 2012
    Posted on April 03, 2012 at 09:45

    Alokm thank you for your reply.

    my confusion about this signal came from the fact that the schematic for stm32-h107 shows that signal VBUSON drives also an external pin. I measured its voltage from curiosity and despair, and the voltage was zero.

    So if i understood correctly, mcu uses the switch and so defines VBUSON in host mode only?