Question
Pin termination normally & after power up STM32
Posted on August 14, 2015 at 12:22
I am using STM32F205 LQFP64 & want to know if below configuration of pin are ok. I use SWD method.I have grouped pins as:
1. vbat: If not used, connect it to Vdd & decouple by 0.1uf cap.2. PA0-PA15: If any of pin is not used, make it internal pull up or output low after power up Except PA13(SWDAT) & PA14(SWCLK).Leave these pins float as they have internal pull-up/down according to datasheet.3. PB0-PB15: If any of pin is not used, make it internal pull up or output low after power up4. PC0-PC15: If any of pin is not used, make it internal pull up or output low after power up. Except PC13, PC14, PC15 as these have alternate function with RTC oscillator & alarm. Should I also make them internal pull up or output low after power up in case not used?5. PD2: if not used, make it internal pull up or output low after power up6. PH0-PH1: Alternate function with main oscillator. Should I also make them internal pull up or output low after power up in case I am using internal oscillator?7. NRST: decouple with 0.1uf cap, it has internal pull-up according to datasheet.8. Vcap1-vcap2: Decouple with 2.2uF cap each.9. VDD1-VDD4, VSS3-VSS4: Decouple each vdd with 0.1uF cap, with additional 4.7uF decouple cap on one vdd.10. VDDA, VSSA: decouple with 0.1uf & 1uf cap.11. Boot: pull down with 10K because code is exceuted form flash.