Skip to main content
Associate II
Feb 27, 2024 8:26 AM UTC
Solved

Pin PC13 in input mode with pull up option does not drive the pin high. STM32F411

Hi,

I am trying to configure the pin PC13 in my STM32F411 device as Input with Pull up option and it is connected to a rotary encoder. At initial bootup time, the pin is in toggle state and after that, it is set to 0. In the same project, I also configured the RTC. This PC13 pin has an alternate function as RTC_AMP1, RTC_OUT, and RTC_TS. Could you please explain the reason for this?

Thanks and Regards

Vrinda R

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 27, 2024 9:31 AM UTC

Hello @vrindar and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you take a look at the errata mentioned on the errata 2.2.10 of the ES0287.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 27, 2024 9:31 AM UTC

Hello @vrindar and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you take a look at the errata mentioned on the errata 2.2.10 of the ES0287.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.