Skip to main content
darshan
Visitor II
November 30, 2015
Question

Pin configuration of SYS_WAKEUp pins when in Standby mode.

Posted on November 30, 2015 at 13:35

Whats the internal resistance of SYS_WAKEUP pin when in standby mode...?

I dont see any info about it in reference manuals..

 

#stm32-power-mod #standby
This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
December 7, 2015
Posted on December 07, 2015 at 11:29

Hi freshflash,

Look to the datasheet of the product you are using (GPIO characteristics) section.

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Visitor II
February 3, 2025

"I am using the STM32G070CB controller and have configured it to interface with the MCP3561 ADC. However, I have disabled adc and still experiencing higher-than-expected current consumption. Below is my configuration. Can you review it and suggest if there are any issues or improvements to reduce power consumption?"

 

sprintf((char*) print,"STANDBY MODE is ON\r\n");

tx_com(print, strlen((char const*) print));

GPIO_InitTypeDef GPIO_InitStruct = { 0 };

 

GPIO_InitStruct.Pin = GPIO_PIN_5;

// GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin = GPIO_PIN_0 ;

// GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin =GPIO_PIN_13;

// GPIO_InitStruct.Mode =GPIO_MODE_ANALOG;

GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_7 | GPIO_PIN_13;

GPIO_InitStruct.Mode =GPIO_MODE_ANALOG;

// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin = GPIO_PIN_15;

GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3

| GPIO_PIN_4 | GPIO_PIN_6 | GPIO_PIN_7 | GPIO_PIN_8

| GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 | GPIO_PIN_13

| GPIO_PIN_14 ;

GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin = GPIO_PIN_8;

GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin =GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3

| GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7

| GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 | GPIO_PIN_15;

GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 

GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3;

GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

// GPIO_InitStruct.Mode =GPIO_MODE_OUTPUT_OD;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

/* Finally enter the standby mode */

__HAL_PWR_CLEAR_FLAG(PWR_SCR_CWUF);

get_time();

 

HAL_Delay(1000);

if (alarm)

{

//to_do_on_alarm();

alarm = 0;

// set_alarm();

}

 

HAL_PWR_EnterSTANDBYMode();