Skip to main content
Associate III
Apr 22, 2025 7:24 AM UTC
Solved

Pin Assignment Issues on STM32H745 with Ethernet, QSPI, and LCD

Hello! I'm creating my own board based on the STM32H745I-DISCO board. I want to use the LQFP208 package of the STM32H745, which has fewer pins than the original package of the DISCO board. I need to connect Ethernet, a display, and QSPI, among other peripherals.

 

I've encountered a conflict where the LCD_DE pin connects to PF10, which is also used by the QSPI_CLK pin. I saw that QSPI_CLK is also available on PB2. However, PB2 is occupied by MII_TX_ERR/nINT

.

My question arises when I notice that this pin is not defined in the Ethernet configuration in MXCube (I'm new to the CubeIDE environment and ST's frameworks, and I'm worried I might be missing something). In fact, I disconnected this pin between the Ethernet driver and the STM32H745, and communication with a test server still works.

 

So my question is: Is it really a good idea to leave the MIIMII_TX_ERR/nINT pin unconnected? Could it be that communication works for now, but if some kind of error occurs, it could cause problems?

 

Thanks, best regards!

This topic has been closed for replies.
TDK
TDKBest answer
Apr 22, 2025 12:59 PM UTC

ETH_TX_ERR is optional for MII and doesn't exist at all for RMII.

LCD_DE is available on PE13. Should be able to have all 3 peripherals active, including TX_ERR if you want it, without conflicts.

TDK_0-1745326759253.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

1 reply

TDK
TDKBest answer
Apr 22, 2025 12:59 PM UTC

ETH_TX_ERR is optional for MII and doesn't exist at all for RMII.

LCD_DE is available on PE13. Should be able to have all 3 peripherals active, including TX_ERR if you want it, without conflicts.

TDK_0-1745326759253.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."