Skip to main content
Antypas.Peter
Senior
September 25, 2019
Question

Phantom external interrupt issue with STM32F469AI (custom board)

I am witnessing interrupts on EXTI9_5 line which have absolutely no electrical stimulus. I'm seeing this behavior consistently on multiple chips so this isn't a one-off.

The GPIO in question (ONE_WIRE_PIN) is PA8.

GPIO initialization here:

mIRQConfig.Pin = ONE_WIRE_PIN;
 mIRQConfig.Mode = GPIO_MODE_IT_FALLING;
 mIRQConfig.Pull = GPIO_NOPULL;
 mIRQConfig.Speed = GPIO_SPEED_FREQ_HIGH;
 HAL_GPIO_Init(ONE_WIRE_PORT, &mIRQConfig);

Here is the interrupt routine:

void EXTI9_5_IRQHandler(void)
 {
 if ( EXTI->PR & ONE_WIRE_PIN )
 {
 HAL_GPIO_EXTI_IRQHandler(ONE_WIRE_PIN);
 }
 else if ( EXTI->PR & POWER_INT_PIN )
 {
 HAL_GPIO_EXTI_IRQHandler(POWER_INT_PIN);
 }
 else if ( EXTI->PR & TOUCH_INT_PIN )
 {
 HAL_GPIO_EXTI_IRQHandler(TOUCH_INT_PIN);
 }
 }

The HAL_GPIO_EXTI_IRQHandler is the vanilla implementation in the HAL:

void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)
{
 /* EXTI line interrupt detected */
 if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)
 {
 __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);
 HAL_GPIO_EXTI_Callback(GPIO_Pin);
 }
}

And my callback is:

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
 {
 switch(GPIO_Pin)
 {
 case TOUCH_INT_PIN:
 {
 ewd1020_touch_int();
 }
 break;
 case POWER_INT_PIN:
 {
 max17043_clear_alert();
 }
 break;
 case ONE_WIRE_PIN:
 {
 singleWireSerialFallingEdge();
 }
 break;
 }
 }

The oscilloscope shows a constant voltage of 1.8V on that pin (VCC), with no falling edge triggering. Pullup resistor is external. Clearly, there is no electrical cause for this interrupt.

The interrupts occur as soon as USART2 becomes active. This is 100% repeatable and reproducible.

What could possibly be causing this? I've been working on this processor for 3 years now and I've seen my share of weirdness, but this takes the cake. Is there any HAL bug or misconfiguration that is even capable of exhibiting this behavior?

 UPDATE:

One possible explanation for this problem might be a corruption of the interrupt vector. This is defined below. What would be a good way to validate the integrity of the vector at run time?

The OS is FreeRTOS 9.

__attribute__ ((section(".isr_vectors"), used))
void (* const g_pfnVectors[])(void) = {
 (void (*)(void))((unsigned long)&__stack_end__),
 ResetISR,
 NMI_Handler,
 HardFault_Handler,
 MemManage_Handler,
 BusFault_Handler,
 UsageFault_Handler,
 (void (*)(void))((unsigned long)&__valid_user_code_checksum),
 Unexpected_Handler,
 Unexpected_Handler,
 Unexpected_Handler,
 SVC_Handler,
 DebugMon_Handler,
 Unexpected_Handler,
 PendSV_Handler,
 SysTick_Handler,
 WWDG_IRQHandler, // Window WatchDog 
 PVD_IRQHandler, // PVD through EXTI Line detection 
 TAMP_STAMP_IRQHandler, // Tamper and TimeStamps through the EXTI line 
 RTC_WKUP_IRQHandler, // RTC Wakeup through the EXTI line 
 FLASH_IRQHandler, // FLASH 
 RCC_IRQHandler, // RCC 
 EXTI0_IRQHandler, // EXTI Line0 
 EXTI1_IRQHandler, // EXTI Line1 
 EXTI2_IRQHandler, // EXTI Line2 
 EXTI3_IRQHandler, // EXTI Line3 
 EXTI4_IRQHandler, // EXTI Line4 
 DMA1_Stream0_IRQHandler, // DMA1 Stream 0 
 DMA1_Stream1_IRQHandler, // DMA1 Stream 1 
 DMA1_Stream2_IRQHandler, // DMA1 Stream 2 
 DMA1_Stream3_IRQHandler, // DMA1 Stream 3 
 DMA1_Stream4_IRQHandler, // DMA1 Stream 4 
 DMA1_Stream5_IRQHandler, // DMA1 Stream 5 
 DMA1_Stream6_IRQHandler, // DMA1 Stream 6 
 ADC_IRQHandler, // ADC1, ADC2 and ADC3s 
 CAN1_TX_IRQHandler, // CAN1 TX 
 CAN1_RX0_IRQHandler, // CAN1 RX0 
 CAN1_RX1_IRQHandler, // CAN1 RX1 
 CAN1_SCE_IRQHandler, // CAN1 SCE 
 EXTI9_5_IRQHandler, // External Line[9:5]s 
 TIM1_BRK_TIM9_IRQHandler, // TIM1 Break and TIM9 
 TIM1_UP_TIM10_IRQHandler, // TIM1 Update and TIM10 
 TIM1_TRG_COM_TIM11_IRQHandler, // TIM1 Trigger and Commutation and TIM11
 TIM1_CC_IRQHandler, // TIM1 Capture Compare 
 TIM2_IRQHandler, // TIM2 
 TIM3_IRQHandler, // TIM3 
 TIM4_IRQHandler, // TIM4 
 I2C1_EV_IRQHandler, // I2C1 Event 
 I2C1_ER_IRQHandler, // I2C1 Error 
 I2C2_EV_IRQHandler, // I2C2 Event 
 I2C2_ER_IRQHandler, // I2C2 Error 
 SPI1_IRQHandler, // SPI1 
 SPI2_IRQHandler, // SPI2 
 USART1_IRQHandler, // USART1 
 USART2_IRQHandler, // USART2 
 USART3_IRQHandler, // USART3 
 EXTI15_10_IRQHandler, // External Line[15:10]s 
 RTC_Alarm_IRQHandler, // RTC Alarm (A and B) through EXTI Line 
 OTG_FS_WKUP_IRQHandler, // USB OTG FS Wakeup through EXTI line 
 TIM8_BRK_TIM12_IRQHandler, // TIM8 Break and TIM12 
 TIM8_UP_TIM13_IRQHandler, // TIM8 Update and TIM13 
 TIM8_TRG_COM_TIM14_IRQHandler, // TIM8 Trigger and Commutation and TIM14
 TIM8_CC_IRQHandler, // TIM8 Capture Compare 
 DMA1_Stream7_IRQHandler, // DMA1 Stream7 
 FMC_IRQHandler, // FMC 
 SDIO_IRQHandler, // SDIO 
 TIM5_IRQHandler, // TIM5 
 SPI3_IRQHandler, // SPI3 
 UART4_IRQHandler, // UART4 
 UART5_IRQHandler, // UART5 
 TIM6_DAC_IRQHandler, // TIM6 and DAC1&2 underrun errors 
 TIM7_IRQHandler, // TIM7 
 DMA2_Stream0_IRQHandler, // DMA2 Stream 0 
 DMA2_Stream1_IRQHandler, // DMA2 Stream 1 
 DMA2_Stream2_IRQHandler, // DMA2 Stream 2 
 DMA2_Stream3_IRQHandler, // DMA2 Stream 3 
 DMA2_Stream4_IRQHandler, // DMA2 Stream 4 
 ETH_IRQHandler, // Ethernet 
 ETH_WKUP_IRQHandler, // Ethernet Wakeup through EXTI line 
 CAN2_TX_IRQHandler, // CAN2 TX 
 CAN2_RX0_IRQHandler, // CAN2 RX0 
 CAN2_RX1_IRQHandler, // CAN2 RX1 
 CAN2_SCE_IRQHandler, // CAN2 SCE 
 OTG_FS_IRQHandler, // USB OTG FS 
 DMA2_Stream5_IRQHandler, // DMA2 Stream 5 
 DMA2_Stream6_IRQHandler, // DMA2 Stream 6 
 DMA2_Stream7_IRQHandler, // DMA2 Stream 7 
 USART6_IRQHandler, // USART6 
 I2C3_EV_IRQHandler, // I2C3 event 
 I2C3_ER_IRQHandler, // I2C3 error 
 OTG_HS_EP1_OUT_IRQHandler, // USB OTG HS End Point 1 Out 
 OTG_HS_EP1_IN_IRQHandler, // USB OTG HS End Point 1 In 
 OTG_HS_WKUP_IRQHandler, // USB OTG HS Wakeup through EXTI 
 OTG_HS_IRQHandler, // USB OTG HS 
 DCMI_IRQHandler, // DCMI 
 CRYP_IRQHandler, // CRYP crypto 
 HASH_RNG_IRQHandler, // Hash and Rng
 FPU_IRQHandler, // FPU
 UART7_IRQHandler, // UART7
 UART8_IRQHandler, // UART8
 SPI4_IRQHandler, // SPI4
 SPI5_IRQHandler, // SPI5
 SPI6_IRQHandler, // SPI6
 SAI1_IRQHandler, // SAI1
 LTDC_IRQHandler, // LTDC
 LTDC_ER_IRQHandler, // LTDC error
 DMA2D_IRQHandler, // DMA2D
 QUADSPI_IRQHandler, // QUADSPI
 DSI_IRQHandler, // DSI
};

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
September 25, 2019

> absolutely no electrical stimulus

Connect it directly to GND to be sure.

JW

Antypas.Peter
Senior
September 25, 2019

Grounding defeats it. But it's supposed to be a falling edge and the scope doesn't detect anything. I've set the threshold to 1.72V with a VCC of 1.8V and it's not triggering on the scope, so why would it trigger inside the GPIO?

waclawek.jan
Super User
September 27, 2019

Maybe because your scope+probe+grounding arrangement is not fast enough to capture short spikes the EXTI pin sees.

JW

Antypas.Peter
Senior
September 27, 2019

Switching from PA8 to PB14 resolved the issue. This will remain a mystery for now.