Peripheral current/power consumption data for STM32L476RG
Dear community,
I am planning on using the STM32L476RG for a project. That project is a low power application, so the current consumption is really important to this project. However I cannot find any reliable source for the current consumption of the peripherals on the L476.
For example, the F407VE has a neat table in its specification (Table 28 in DS8626) where the typical current consumption for all peripherals is given. It's a great way to estimate the total current consumption in a system in the planning phase of a project. The only thing I could find in this regard is chapter 6.3.5 "Supply current characteristics" in DS10198. Problem is: the supply currents listed there are only given for the case that all peripherals are off. I can't derive my total current consumption from that if I plan to use a UART, a timer, an ADC and so on.
However, I could not find such a table for the L476RG, which is... odd, to say the least. Since the L series is advertised as a low power controller I would expect that one can find such parameters in the datasheets expecially for the L series.
Did I miss something? Can I find similar data for the L476?
Thank you advance.