Skip to main content
luisf
Associate II
November 10, 2017
Question

Perform Smooth Calibration on STM32L433 not working

Posted on November 10, 2017 at 21:03

Hi, 

I need to calibrate my RTC crystal that is drifting about 7 seconds every 18014 that according to my calculations is about 389 ppm. I Tryed to perform the calibration with the following initialization code, but regardless of the HAL_RTCEx_SetSmoothCalib function, the drift is the same. Is there any special procedure to proper perform the calibration?

static void rtc_config(void)

{

hrtc.Instance = RTC;

if(hrtc.Instance->ISR & RTC_ISR_INITS)

{

   hrtc.Init.HourFormat = RTC_HOURFORMAT_24;

   hrtc.Init.AsynchPrediv = 127;

   hrtc.Init.SynchPrediv = 255;

   hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;

   hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;

   hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;

   hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;

   if (HAL_RTC_Init(&hrtc) != HAL_OK)

   {

      Error_Handler();

   }

   /* Get the RTC current Time */

   rtc_get_real_time();

   if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 2048, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)

   {

      //Error_Handler();

   }

}

else

{

   MX_RTC_Init();

   /* Get the RTC current Time */

   rtc_set_time(946684800);

}

while(hrtc.Instance->ISR & RTC_ISR_INITF);

HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, RTC_SMOOTHCALIB_PLUSPULSES_SET, 133);

}

Thank you for the help;

    This topic has been closed for replies.