Question
Parsing ETH/RS232<->CAN
Posted on September 18, 2017 at 16:31
Hi community,
i have following situation:
PC <--- ETH or RS232 ----> STM32F107 < ----CAN---- > STM32F105 with external power module
I want to parse the ascii message (example K01NC|200) to a smaller protocol what i can send via CAN-Bus at once (max 8 Byte). Maybe to '0xA3' .
When the STM32F105 has the work finished the work, a echo should be send back to the pc. So the F107 has to translate the echo from the F105 ('0xA3' to 'K01NC|200') and send it back to the pc.
Is there any parser what is already finished and can manage that ?
There are to many commands, so that i dont want to check via switch/case....