Skip to main content
majd-ghadab
Associate II
September 25, 2019
Question

Parallel SDRAM

  • September 25, 2019
  • 1 reply
  • 891 views

Hello everyone, i would like to connect STM32F7 with multiple SDRAMs because i would like to get at least 256 MByte, i spent too much time trying to search for a detailed way, how to connect at first more thant one SDRAM together and then to connect them with STM32F7. but i couldn't find out. can someone please provide me with these informations.

Thanks.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 26, 2019

It supports TWO banks, one at 0xC0000000 the other at 0xD0000000

As I recall the interface to both is the same, but there are two chip select signals SDNE[1:0] and two clock enables SDCKE[1:0]

I'm sure this is covered in one of the Reference Manuals

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..