Question
Output of STM32F100RB DiscoveryVL board when connected to 3v3 converter only shows from 2.58 to 3.19 volts on the input and alway 5v on the output of converter.
I have a Value Line Discovery board - STM32F100RB and three of the outputs are connected to a 3v3 converter to get a 5v output. I have tried another controller board with 3v3 outputs to drive the convertor board and I get a clean signal. (Either 0 or 5v). I am using STM32CubeMX to generate the code and compiling it on True Studio. I have tried setting the configuration of the pin to: GPIO_NOPULL, GPIO_PULLUP and GPIO_PULLDOWN.
I have posted the code up on github at htpps://github.com/sunbelt56/DiscoveryVL.git