Skip to main content
Kang Sung Gu
Associate II
September 18, 2017
Question

Output control Question

  • September 18, 2017
  • 2 replies
  • 530 views
Posted on September 18, 2017 at 02:59

0690X00000608HJQAY.png

EX) ODR = 1   -> I/O Pin State = 0 ?

It is True?

If ODR = 1 then I / O port is also 1?

Is it OutputControl Not Gate?

    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    September 18, 2017
    Posted on September 18, 2017 at 08:22

    It's more a block diagram and not a true schematics.

    If ODR=1, unless given pin is set to open-drain in OTYPER,  the PMOS is switched on, ie. on output you will see log.1.

    If ODR=0, NMOS is switched on ie. output is set to 0.

    JW

    Kang Sung Gu
    Associate II
    September 18, 2017
    Posted on September 18, 2017 at 08:53

    Thank you for a detailed description