Output Capture not working to blink LED on NUCLEO-C031C6
I am trying to implement output capture using the LL APIs but cannot get it to blink the LED every one second on the NUCLEO board, however, I cannot get it to blink at all. Is there a register I missed?
Here is my code:
#include "stm32c0xx_ll_bus.h"
#include "stm32c0xx_ll_gpio.h"
#include "stm32c0xx_ll_tim.h"
/*---------------------------------------------------------------------------------------------------------------------------------------------------*/
void LED_PA5_init(void)
{
LL_IOP_GRP1_EnableClock (LL_IOP_GRP1_PERIPH_GPIOA); //for LED PA5
LL_GPIO_SetPinMode (GPIOA, LL_GPIO_PIN_5, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetAFPin_0_7 (GPIOA, LL_GPIO_PIN_5, LL_GPIO_AF_5); //AF5 is TIM1_CH1 for PA5
}
void Timer1_1Hz_OC_init(void) //1 Hz = 1 cycle/s = 1 s delay
{
LL_APB2_GRP1_EnableClock (LL_APB2_GRP1_PERIPH_TIM1);
LL_TIM_SetPrescaler (TIM1, 1200-1); //12000000/1200 = 10000 Hz
LL_TIM_OC_SetMode (TIM1, LL_TIM_CHANNEL_CH1, LL_TIM_OCMODE_TOGGLE);
LL_TIM_CC_EnableChannel (TIM1, LL_TIM_CHANNEL_CH1);
LL_TIM_SetAutoReload (TIM1, 10000-1); //10000/10000 = 1 Hz
LL_TIM_SetCounter (TIM1, 0);
LL_TIM_EnableCounter (TIM1);
}
/*---------------------------------------------------------------------------------------------------------------------------------------------------*/
int main(void)
{
LED_PA5_init();
Timer1_1Hz_OC_init();
while (1){ }
}