Skip to main content
Associate III
April 18, 2025
Question

OTA IN STM32U575 USING ESP32

  • April 18, 2025
  • 8 replies
  • 1102 views

IS ANY BODY HELP ME IN THE OTA OF THE STM32U575 USING THE ESP32

1. HOW TO SETUP THE SYSTEM BOOTLOADER TO RECEIVE THE FIRMWARE (.BIN FILE) VIA UART AND HOW TO SELECT WHICH UART TO USE FOR UPLOAD , THERE ARE MORE UART WHICH SUPPORT THE UART FLASHING HOW TO ACTIVATE THE DESIRED UART FOR THE FIRMWARE UPLOAD

2. PLEASE SHARE ME ANR RESOUSE REGARDING SYSTEM BOOTLOADER CONFIGURATIONS

3. PLEASE SHARE ANY ESP32 FIRMWARE TRANSMIT THE BINARY FILE VIA UART

This topic has been closed for replies.

8 replies

Andrew Neil
Super User
April 18, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
premkumarAuthor
Associate III
April 18, 2025

sorry for that
in stm32u575

              Will you help me ,how the system bootloader works , how to activate that and how to receive the firmware via usart and selecting the uart for the firmware is ther any configuration  

Tesla DeLorean
Guru
April 18, 2025

AN2606 describes the pins involved. Shows the UART Rx pins. You send an 0x7F data pattern at baud rate with 8E1 format for it to auto baud.

AN3155 describes the protocol after you reset with BOOT0  HIGH.

See examples on Arduino MKR WAN1300 Github 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..