OpenOCD failed : stm32f4x.cfg:77: Error: invalid subcommand "newtap stm32f412 cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id 0x4ba00477"
Hi experts,
We have created a project on WICED 43xx_Wi-Fi sdk for STM32F412 MCU+43438 wlan chip.
We have connected st-link V2 debugger to the EVB and we could see "STM32 STLink" in windows Device Manager.
When we used openOCD to flash debugger to EVB, it would show below error:
Here comes the command and terminal output that we used to programming.
****************************************************************************
C:\Users\wayne\Documents\WICED-Studio-6.3\43xxx_Wi-Fi>tools\OpenOCD\Win32\openocd-all-brcm-libftdi.exe -s tools\OpenOCD\scripts -f tools\OpenOCD\stm32f412discovery.cfg -f tools\OpenOCD\stm32f4x.cfg
Open On-Chip Debugger 0.10.0+dev-00227-g0d15c62 (2018-03-27-15:19)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 2000 kHz
adapter_nsrst_delay: 100
none separate
srst_only separate srst_nogate srst_open_drain connect_deassert_srst
adapter speed: 1000 kHz
adapter_nsrst_delay: 100
tools\OpenOCD\stm32f4x.cfg:77: Error: invalid subcommand "newtap stm32f412 cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id 0x4ba00477"
in procedure 'script'
at file "embedded:startup.tcl", line 60
in procedure 'jtag' called at file "tools\OpenOCD\stm32f4x.cfg", line 77
****************************************************************************
Please help for clarifying this issue and if need anything information please let me know.
Your help will be appreciated.
Thanks.
BR,
Wayne