Skip to main content
Hedley
Associate III
Dec 9, 2019 2:45 AM UTC
Question

Openocd

I ported openocd to the stm32l522. ​

​

https://github.com/morbos/openocd-0.10.1

​

openocd -f board/st_nucleo_l522.cfg​

​

From there you can remote connect from gdb, flash, and see the s/ns processor regs. Watchpoints work also.

​

Hedley​

​

This topic has been closed for replies.

3 replies

TarekB-ST
Associate
Dec 20, 2019 5:23 PM UTC

Nice!

I suggest to post your change into the official OpenOCD repository.

There a whole gerrit to review changes at: http://openocd.zylin.com

By the way, for STM32L5 there is already an existing change at : http://openocd.zylin.com/#/c/5344

You can try to find a consensus with the owner of the change, if you judge that your change is more appropriate.

Happy New Year !

Tarek

Hedley
HedleyAuthor
Associate III
Dec 20, 2019 6:26 PM UTC

Hi Tarek,

Appreciate the code ptr. That version supports L5 as a new flash target. I do also. The missing piece is ARMv8m support. I handle the secure and non secure contexts. That also involved a change to the STlink hla code to make it ARMv8m aware.

​

Enjoy the Festive Season​!

​

Hedley

Hedley
HedleyAuthor
Associate III
Jan 2, 2020 10:26 PM UTC

I updated the openocd me. It's st_nucleo_l552.cfg dunno why I have been typoing that as 522...

​

The new version also supports correct flash size reading and flashing when the watermarks are used. ​before, if you watermark the S/NS split, the erase fails at the watermark address. The soln I found was to temporarily unlock the option bytes and default the watermarks, I dont permanently write them, it's just for the curr reset. Next time you reset, the old values take over.

​

I have 2 Ada programs running on the stm32l552. The first part of the flash at 0C000000 is S, then at the watermark, the NS program begins at 0802xxxx.

​

There is no ST sample code so I had to do this blind with just the RM and SVD file + prior L4 ports.​

​

github.com/morbos/STM32/tree/master/L/L552/sx1276_rom_l552​