Skip to main content
JustMe
Associate II
February 26, 2019
Question

Op Amp to ADC 'spair' pins not available for other use??

  • February 26, 2019
  • 0 replies
  • 442 views

STM32F302RBT...

I want to use OpAmp1 in PGA Connected mode feeding ADC1 IN3. According to CubeMX the OpAmp pins VINP, OPAMP_VOUT and VINM are all 'Used' even though VOUT is internally connected to the ADC and VINM is not being used.

If in the cube I change the setting of VINM to GPIO it shows that the opamp to adc connection is no longer available.

Is this just an error in CubeMX or are those pins no longer available for other use?

    This topic has been closed for replies.