Skip to main content
hg-chen
Associate III
August 7, 2008
Question

only one breakpoint can be set?

  • August 7, 2008
  • 2 replies
  • 779 views
Posted on August 07, 2008 at 05:49

only one breakpoint can be set?

    This topic has been closed for replies.

    2 replies

    hg-chen
    hg-chenAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    This question should be related to IAR EWARM,

    but I do not know the place of the IAR forum,

    the question is while enter debugging,

    the message below shown, or refer to attached file.

    The C-SPY option ''Run to 'main''' is enabled,but due to a lack of

    breakpoints this will require single-stepping ,which may take a long

    time.

    Do you want to execute anyway,or stop at the first instruction?

    only one breakpoint can be set under this condition!

    why and how to get it right?

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    which device are using(STM32, STR9,..)? BTW with the STM32 you can set more than 2 breakpoints.