Skip to main content
Associate
Sep 27, 2025 1:58 AM UTC
Question

Only 16K of 8M PSRAM accessible on B-U585I-IOT02A

I'm using a B-U585I-IOT02A board and the IOT_HTTP_WebServer example code. 

My read is the PSRAM is 8M on that board, but I can only access 16K (to 0x2803ffff) and then ???? is not IDE memory display or a trap in the code.  Is this a CPU configuration issue?

 

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
Sep 30, 2025 9:54 AM UTC

Hello @Marty ;

 

Could you please check the device size?

hospi1.Init.DeviceSize = 23;

 

Also, I recommend you to look at OSPI_PSRAM_MemoryMapped example and check the OCTOSPI configuration.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.