Skip to main content
SSmit.0
Associate III
October 11, 2018
Question

One pulse mode internal trigger

  • October 11, 2018
  • 2 replies
  • 3973 views

Hi,

I'm currently trying to create a software pulse for an ADC with an stm32 device which I'm pretty new to.

I have everything working and receive data clocked via HAL_SPI_Receive, but the pulse is created via a hardware trigger and this is the only configuration I can find regarding one pulse mode. 

This is the ADC I am using

http://www.analog.com/media/en/technical-documentation/data-sheets/231116fa.pdf

I am trying to generate the CNV/acquisition pulse. 

I want to call a function or set a bit, etc, which internally triggers a defined pulse for the CNV pin, something similar to HAL_TIM_OC_Start()

After this I will use HAL_SPI_Receive to clock through the data and do a few other things before wanting to initiate the next pulse.

At the moment the trigger is generated though a channel on TIM1, with PWM generation on CH2 and slave mode set as trigger mode with TI1FP1 as trigger source and clock source set to internal. I can create what ever pulse I like using a hard trigger on associated pin but I want to replace this with a software call. Or alternatively achieve the same outcome, i.e a pulse, some other way. I am new to STM programming and am working with others unfamiliar with coding so want to use the HAL if possible. 

Thanks

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
October 12, 2018

> At the moment the trigger is generated though a channel on TIM1, with PWM generation on CH2 and

> slave mode set as trigger mode with TI1FP1 as trigger source and clock source set to internal. I can

> create what ever pulse I like using a hard trigger on associated pin but I want to replace this with a

> software call.

Simply enable the timer, by setting TIMx_CR1.CEN. This is the same what the slave-mode controller does when a trigger pulse arrives, when the slave-mode controller is set to trigger mode.

> want to use the HAL if possible.

I don't Cube/HAL, but in [STM32Cube_FW_F4_V1.15.0]\Drivers\STM32F4xx_HAL_Driver\Inc\stm32f4xx_hal_tim.h I see:

#define __HAL_TIM_ENABLE(__HANDLE__)                ((__HANDLE__)->Instance->CR1|=(TIM_CR1_CEN))

(the comment above it, saying " * @brief Enable the TIM peripheral.", is of course incorrect, as this enables only the counter within TIM, not TIM as such).

JW

SSmit.0
SSmit.0Author
Associate III
October 14, 2018

Hi,

Thanks for the response, I have got software pulse triggering working using "__HAL_TIM_ENABLE(&htim1)". 

I have a problem with using it in the code below. 

HAL_TIM_OnePulse_Start(&htim1, TIM_CHANNEL_1);
volatile uint16_t array [300];
HAL_Delay(1000); 		// let ADC power up
		
while(1)
 		{
	 	for(int n=0;n<300;n++) 				// acquisition loop
			{
				if (hspi1.State != HAL_SPI_STATE_BUSY_RX)
				{
					__HAL_TIM_ENABLE(&htim1);	//send pulse	
		HAL_SPI_Receive(&hspi1,(uint8_t*)array[n],1,1);	//clock data
					HAL_Delay(1);
				}
			}
		}

With the HAL_Delay(1); in the loop, the pulses look fine but for some reason the HAL_SPI_Receive function isn't initiated - there are no clocks. When I remove the delay, the clock is there but the pulse output is almost inverted being high most of the time, and even runs over the receive clock? 

I don't quite understand what's going on as I have the != HAL_SPI_STATE_BUSY_RX there but I don't think it's working?

Thanks