Skip to main content
Senior
Sep 4, 2023 6:16 AM UTC
Solved

One bit shift in SPI communication on STM32G4

Hi,

I am working on SPI communication between STM32G491 and ATM90E26. and I am using the SPI polling API with HAL_SPI_Transmit and HAL_SPI_Receive.

My System clock is 96Mhz and I am using prescaler of 64 for SPI.

CLKPolarity=Low,

CLKPhase=1Edge.

Communication is happening between the devices but I am not getting the correct data.
there is only a shift of one bit.

For example
in binary:

expected: 0001 0011 1001 0100

received: 0000 1001 1100 1010
f I shift the received bitstream to the left I get exactly the right result.

I found one solution in the forum for similar type of question(for stm32H7) It was solved with
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;

But I am using STM32G4 with SPI Poll method
there is no MasterKeepIOState parameter  available its giving me the error I use it.
Is it due to bad configutation?

or anything do I need to configure to solve it. Can anyone please suggest.

Thanks

 

 

This topic has been closed for replies.
David Littell
David LittellBest answer
Senior II
Sep 5, 2023 3:04 PM UTC

Note that SPI is a bit exchange protocol.  For every bit you send you receive a bit.  So, given the "SPI sequence" you show you must transmit 3 bytes in order to properly set the register address and transfer the 2 data bytes (for either a read or write operation).  You must use a 3-byte HAL_SPI_TransmitReceive() for the register read operation.

9 replies

Issamos
Super User
Sep 4, 2023 6:49 AM UTC

Hello @sireevenkat1

I suggest you to try to compare your exemple to one of those exemples.

Else, you can take a look at the UM2570 to find all SPI commands.

Best regards

II

David Littell
Senior II
Sep 4, 2023 12:46 PM UTC

Normally this problem is due to a SPI clock signal integrity issue.  Ensure the SPI clock is clean with minimal switching artifacts, reflections, etc.

Senior
Sep 5, 2023 4:36 AM UTC

Thanks for the replies @David Littell @Issamos ,

I changed SPI prescaler from 64 to 256 ,Now I can able to read correct values from few registers(ATM90E26 is energy meter IC).Now I can able to read frequency & meter status registers correctly. But If I read voltage and current registers I am always getting value zero values.
In ATM90E26 datasheet SPI Interface Bit Rate  max is 160K Bps.

In my configuration 96Mhz(system clock)/256(prescaler)=375 kbps.
Is the issue with Bit rate? Can anyone clarify me ?
Because I can able to read few registers of ATM90E26 correctly & few registers I can't able to read.
Thanks

Issamos
Super User
Sep 5, 2023 6:49 AM UTC

Hello again

I suggest you to reduce your bit rate and retry.

Best regards.

II

Senior
Sep 5, 2023 7:21 AM UTC

Hi,

I did that still same issue.
Thanks

David Littell
David LittellBest answer
Senior II
Sep 5, 2023 3:04 PM UTC

Note that SPI is a bit exchange protocol.  For every bit you send you receive a bit.  So, given the "SPI sequence" you show you must transmit 3 bytes in order to properly set the register address and transfer the 2 data bytes (for either a read or write operation).  You must use a 3-byte HAL_SPI_TransmitReceive() for the register read operation.

Visitor II
Dec 24, 2023 1:09 PM UTC

Try enabling the SPI unit before selecting the slave